Hello,
I have successfully configured and installed LTIB.
uImage, kernel and filesystem have been created.
Now i transferred uImage and kernel on SD-Card, when i started the board, it shows following.
=====================================================================================
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: ncq stag pm led clo only pmp pio slum part
No port device detected!
** Bad device size - sata 0 **
** Bad device size - sata 0 **
SATA device 1: unknown device
** Bad device sata 1 **
** Bad device sata 1 **
MMC: no card present
mmc0(part 0) is current device
MMC: no card present
** Bad device mmc 0 **
MMC: no card present
** Bad device mmc 0 **
mmc1 is current device
** Unrecognized filesystem type **
Failed to mount ext2 filesystem...
** Unrecognized filesystem type **
(Re)start USB...
USB0: lowlevel init failed
USB1: USB EHCI 1.00
scanning bus 1 for devices... 2 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found
scanning usb for ethernet devices... 0 Ethernet Device(s) found
USB device 0: unknown device
** Bad device usb 0 **
** Bad device usb 0 **
USB device 1: unknown device
** Bad device usb 1 **
** Bad device usb 1 **
6x_bootscript not found
serial console at 115200, 8N1
details at http://boundarydevices.com/6q_bootscript
========================================================================================
Can anyone please tell me what the problem is? How should i transfer the images? Or Any configuration I am missing?