Hi ,
I am working over the IMX6 based custom target prototype board. I need to validate all the interfaces like I2C , SPI etc
on the board. Does NXP provides any solution to test the bare board ?
Just want to know the possible solutions to test the bare board( Not having any boot loader and kernel) . Please suggest.
Regards,
Aditya Nagal
Hello,
You may try using the i.MX6 Platform SDK. Bare-metal SDK for the i.MX 6 series, includes
reusable drivers and tests for many peripherals, and much example code. Also includes register
definition headers files, and register definitions for debuggers.
The SDK contains the following documentation :
iMX6_Platform_SDK\README.pdf — very useful and should be read first.
iMX6_Platform_SDK\doc\iMX6_Firmware_Guide.pdf - «provides example driver code,
that demonstrates the proper initialization, boot up and basic I/O operation of i.MX 6
peripherals and controllers. This code can be implemented into test suites or boot code
to help ensure proper board functionality».
iMX6_Platform_SDK\doc\Platform SDK Build System Architecture.pdf —contains general details
about examples building.
swp-report/iMX6_Platform_SDK at master · backenklee/swp-report · GitHub
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------