How to split two HDMI display to two OS using Jailhouse hypervisor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to split two HDMI display to two OS using Jailhouse hypervisor

2,027 Views
hongxingyu1982
Contributor III

Hi ,sir

 

    I am using  GPU + first hdmi(DCSS->HDMI) + second hdmi (LCDIF->DSI->HDMI) on mx8mq yocto.  How to move the second hdmi LCDIF->DSI->HDMI use from yocto ? I plan to run two Linux OS using Jailhouse hypervisor, OS1 used GPU + first hdmi(DCSS->HDMI), OS2 used second hdmi (LCDIF->DSI->HDMI). 

     How could I change the dts files or other files ?

     Any suggestion are welcome!

0 Kudos
Reply
3 Replies

1,907 Views
vsuneja63
Contributor III

Hi Hongxing Yu,

Did you get the solution for this? I am trying to achieve the same via jailhouse hypervisor on imx8mqevk. Please share if you resolved this.

Thanks & Regards,

Vipul Kumar

0 Kudos
Reply

1,907 Views
b36401
NXP Employee
NXP Employee

I can suggest to manage whole screen with X-server running on one OS and open X window on part of the screen with remote client.

0 Kudos
Reply

1,907 Views
hongxingyu1982
Contributor III

Hi everyone

Could you support some suggestion ?

Thanks

BR

0 Kudos
Reply