How to split two HDMI display to two OS using Jailhouse hypervisor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to split two HDMI display to two OS using Jailhouse hypervisor

2,009 次查看
hongxingyu1982
Contributor III

Hi ,sir

 

    I am using  GPU + first hdmi(DCSS->HDMI) + second hdmi (LCDIF->DSI->HDMI) on mx8mq yocto.  How to move the second hdmi LCDIF->DSI->HDMI use from yocto ? I plan to run two Linux OS using Jailhouse hypervisor, OS1 used GPU + first hdmi(DCSS->HDMI), OS2 used second hdmi (LCDIF->DSI->HDMI). 

     How could I change the dts files or other files ?

     Any suggestion are welcome!

0 项奖励
回复
3 回复数

1,889 次查看
vsuneja63
Contributor III

Hi Hongxing Yu,

Did you get the solution for this? I am trying to achieve the same via jailhouse hypervisor on imx8mqevk. Please share if you resolved this.

Thanks & Regards,

Vipul Kumar

0 项奖励
回复

1,889 次查看
b36401
NXP Employee
NXP Employee

I can suggest to manage whole screen with X-server running on one OS and open X window on part of the screen with remote client.

0 项奖励
回复

1,889 次查看
hongxingyu1982
Contributor III

Hi everyone

Could you support some suggestion ?

Thanks

BR

0 项奖励
回复