How to solve timing margin issues from fabrication side in custom hardware design ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to solve timing margin issues from fabrication side in custom hardware design ?

4,006 Views
peteramond
Contributor V
Hi All,
This is regarding i.MAX6Q based custom hardware design and I'm having timing margin issues in I/O interface between chipset and dram. If I/O interface margin is poor by routing issue or layout, it may cause failure depending on noise pattern ( different application make different noise  level). So to solve this issue what do you suggest ?
1) Can we do this using chipset design option to control this kind of timing like phase shift  for tDQS and tDQ.? Can you explain how to do this ?
2) Is it possible to down operating frequency ( ex 2400Mbps --> 2133Mbps ) How can we do this in uboot level ?
3) If it is related to clock timing, We can add capacitance or change termination resistance on CLK and CLK/. To do this what we should do ? Which parameter should I change in DDR initialization script before do memory calibration ?
 
Regards,
Peter.
Labels (4)
3 Replies

3,799 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

1.3. please look on AN4467 i.MX 6 Series DDR Calibration

https://www.nxp.com/docs/en/application-note/AN4467.pdf 

2. for changing frequency examples one can look at linux cpufreq, bus drivers described in

Chapter 23 CPU Frequency Scaling (CPUFREQ) Driver, Chapter 24 Dynamic Bus Frequency Driver

attached Linux Manual. For boot with lower frequencies one can use BT_FREQ=1 option

described in Table 8-4. Normal frequency clocks configuration  i.MX6DQ Reference Manual

https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,799 Views
peteramond
Contributor V

Hi igorpadykov

How can I change BT_FREQ=1 value ? Is that in U-boot DCD configuration files ? Could you please tell me the method ?

Regards,

Peter.

0 Kudos
Reply

3,799 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

please look at BT_FREQ (BOOT_CFG3[2]) description in

Table 8-2. Boot eFUSE descriptions, Table 8-3. GPIO override contact assignments

i.MX6DQ Reference Manual.

Best regards
igor

0 Kudos
Reply