I want to test the function which is yuyv to convert to RGB32 in 3.10.53 kernel. But I found the output picture is seprate more picture, and this picture is blurred.
Could you help me to see it?
The G2D convert code as following:
struct g2d_surface src, dst;
struct g2d_buf *buf;
void *handle = NULL;
int size = 640 * 480;
| ret = g2d_open(&handle); |
if(ret < 0) {
| printf("g2d open fail for the ivicar\n"); | |
| return 0; |
}
buf = g2d_alloc(size * 2, 1);
memcpy(buf.buf_vaddr, buf_yuyv, size * 2);
src.planes[0] = buf.buf_paddr;
src.left = 0;
src.top = 0;
src.right = 640;
src.bottom = 480;
src.stride = 640;
src.width = 640;
src.height = 480;
src.rot = G2D_ROTATION_0;
src.format = G2D_YUYV;
dst.planes[0] = g_fb_phys;
dst.left = 0;
dst.top = 0;
dst.right = 640;
dst.bottom = 480;
dst.stride = 640;
dst.width = 640;
dst.height = 480;
dst.rot = G2D_ROTATION_0;
dst.format = G2D_RGBA8888;
g2d_blit(handle, &src, &dst);
g2d_finish(handle);
usleep(1000);
g2d_close(handle);
g2d_free(buf);
Hi igorpadykov,
Thanks your advise, But I try scale the image with g2d plugin in the gstreamer-imx, The error information as the following:
# gst-language-1.0 videotestsrc ! video/x-raw,foramt=BGRA,width=640,height=480 ! imxg2dvideotransform ! video/x-raw,width=400,height=240 ! imxipuvideosink
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
g2d_blit: Invalid dst rect, left 0, top 0, right 0, bottom 0, width 400, height 240, stride 400!
ERROR: from element /GstPipeline:pipeline0/GstVideoTestSrc:videotestsrc0: Internal data flow error.
Additional debug info:
/work/yocto/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0/git-r0
/git/libs/gst/base/gstbasesrc.c(2933): gst_base_src_loop (): /GstPipeline:pipeline0/GstVideoTestSrc:
videotestsrc0:
streaming task paused, reason error (-5)
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...
Hi bobo
for conversion example one can try
imxvideoconvert_g2d plugin, check sect.7.5.4 Video Conversion attached Linux Guide
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------