How to program the BOOT_CFG1[7:4] eFUSEs to select the boot device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to program the BOOT_CFG1[7:4] eFUSEs to select the boot device

1,373件の閲覧回数
adityanagal
Contributor III

Hi ,

I am working on the IMX6 solo based target board. I need to select the external boot device. So how to program  BOOT_CFG1[7:4] eFUSEs to select the boot device . Do we need JTAG or some other hardware tool to program these fuses. Please provide the details. Thanks!

Regards,

Aditya Nagal

0 件の賞賛
返信
1 返信

955件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

fuses can be blown in uboot:

https://community.freescale.com/docs/DOC-95458

http://boundarydevices.com/fuse-command/

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信