SDK:Android Q10.0.0_2.2.0_AUTOCurrently using USB3.0 by default, now I want to change to another usb2.0 port。
I will try it on my board this week and then tell you the result.
Do you mean you use the usb otg port in the base board?
yes
The download method is the same, here you need to connect the USB OTG port firstly. If it can not work contact us.
My test failed.
Stuck here:
which version android BSP are you using? And are you using the i.MX8QXP C0 version board?
SDK:Android Q10.0.0_2.2.0_AUTO
I used the development board B0 to test.
https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-8quadxplus...