How to load Falcon mode image to emmc on imx8mplus dev board nxp?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to load Falcon mode image to emmc on imx8mplus dev board nxp?

ソリューションへジャンプ
5,222件の閲覧回数
vivek338
Contributor IV

Hi,

 

Iam following falcon mode document AN14093 rev.2.0 to apply fast boot falcon mode on imx8mplus dev board nxp.

Its working on sd card using below commands to upload in sd card:-

sudo dd if=imx-image-fastboot-imx8mpevk-fastboot.rootfs-20241212111237.wic of=/dev/sda bs=4M status=progres

Now I want to load and boot from emmc on chip on imx8mplus dev board nxp.

How to do that?

 

Thanks in advance !

ラベル(1)
0 件の賞賛
返信
1 解決策
5,173件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Should probably add default bootloader, try below way.

uuu -b emmc_all <default_bootloader> imx-image-fastboot-imx8mpevk-fastboot.rootfs-20241212111237.wic

uuu -b emmc <default_bootloader> <falcon_mode_bootloader>

 

Regards

Harvey

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,193件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Have you tried with the one: uuu -b emmc_all imx-image-fastboot-imx8mpevk-fastboot.rootfs-20241212111237.wic

Regards

Harvey

0 件の賞賛
返信
5,190件の閲覧回数
vivek338
Contributor IV
Hi,
Thanks for replying !
Yes I have tried but got below error :-

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172

Success 0 Failure 1


1:93 1/ 1 [HID(W):LIBUSB_ERROR_TIMEOUT ] SDPS: boot -scanterm -f imx-image-fastboot-imx8mpevk-fastboot.rootfs-20241218045957.wic -scanlimited 0x800000
0 件の賞賛
返信
5,174件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Should probably add default bootloader, try below way.

uuu -b emmc_all <default_bootloader> imx-image-fastboot-imx8mpevk-fastboot.rootfs-20241212111237.wic

uuu -b emmc <default_bootloader> <falcon_mode_bootloader>

 

Regards

Harvey

0 件の賞賛
返信