How to load Falcon mode image to emmc on imx8mplus dev board nxp?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to load Falcon mode image to emmc on imx8mplus dev board nxp?

跳至解决方案
5,442 次查看
vivek338
Contributor IV

Hi,

 

Iam following falcon mode document AN14093 rev.2.0 to apply fast boot falcon mode on imx8mplus dev board nxp.

Its working on sd card using below commands to upload in sd card:-

sudo dd if=imx-image-fastboot-imx8mpevk-fastboot.rootfs-20241212111237.wic of=/dev/sda bs=4M status=progres

Now I want to load and boot from emmc on chip on imx8mplus dev board nxp.

How to do that?

 

Thanks in advance !

标签 (1)
0 项奖励
回复
1 解答
5,393 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Should probably add default bootloader, try below way.

uuu -b emmc_all <default_bootloader> imx-image-fastboot-imx8mpevk-fastboot.rootfs-20241212111237.wic

uuu -b emmc <default_bootloader> <falcon_mode_bootloader>

 

Regards

Harvey

在原帖中查看解决方案

0 项奖励
回复
3 回复数
5,413 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Have you tried with the one: uuu -b emmc_all imx-image-fastboot-imx8mpevk-fastboot.rootfs-20241212111237.wic

Regards

Harvey

0 项奖励
回复
5,410 次查看
vivek338
Contributor IV
Hi,
Thanks for replying !
Yes I have tried but got below error :-

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172

Success 0 Failure 1


1:93 1/ 1 [HID(W):LIBUSB_ERROR_TIMEOUT ] SDPS: boot -scanterm -f imx-image-fastboot-imx8mpevk-fastboot.rootfs-20241218045957.wic -scanlimited 0x800000
0 项奖励
回复
5,394 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Should probably add default bootloader, try below way.

uuu -b emmc_all <default_bootloader> imx-image-fastboot-imx8mpevk-fastboot.rootfs-20241212111237.wic

uuu -b emmc <default_bootloader> <falcon_mode_bootloader>

 

Regards

Harvey

0 项奖励
回复