How to keep imx7d boot logo from uboot to kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to keep imx7d boot logo from uboot to kernel

1,835 Views
864535720
Contributor II

Hello everyone
my development board is IMX7DSABRE. Linux kernel version is 4.9.88.
In the uboot stage, we have implemented the logo display, and in the kernel stage, we have also implemented the logo display, but now we want to keep the logo from uboot to the kernel. The imx6 logo has been continuously displayed in the forum. I read the corresponding patch and found that it is very different from the imx7 implementation. Is there any imx7 logo patch? If not, can you provide some ideas for implementation?
Thank you.

Labels (5)
0 Kudos
Reply
1 Reply

1,773 Views
igorpadykov
NXP Employee
NXP Employee

Hi 其东 刘

I am afraid such patches are not available, available only for i.mx6:

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply