How to install the fsl codec on linux?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to install the fsl codec on linux?

2,494 Views
taverdetagnès
Contributor I

Hi, I use gst-streamer-1.8.1 and gst1-imx-0.12.0

I installed those plugins

# gst-inspect-1.0 | grep imx
imxvpu: imxvpuenc_mjpeg: Freescale VPU motion JPEG video encoder
imxvpu: imxvpuenc_mpeg4: Freescale VPU MPEG-4 video encoder
imxvpu: imxvpuenc_h264: Freescale VPU h.264 video encoder
imxvpu: imxvpuenc_h263: Freescale VPU h.263 video encoder
imxvpu: imxvpudec: Freescale VPU video decoder
imxg2d: imxg2dcompositor: Freescale G2D video compositor
imxg2d: imxg2dvideotransform: Freescale G2D video transform
imxg2d: imxg2dvideosink: Freescale G2D video sink
imxpxp: imxpxpvideotransform: Freescale PxP video transform
imxpxp: imxpxpvideosink: Freescale PxP video sink
imxeglvivsink: imxeglvivsink: Freescale EGL video sink
imxaudio: imxuniaudiodec: Freescale i.MX uniaudio decoder
imxv4l2videosrc: imxv4l2videosrc: V4L2 CSI Video Source
imxipu: imxipucompositor: Freescale IPU video compositor
imxipu: imxipuvideosink: Freescale IPU video sink
imxipu: imxipuvideotransform: Freescale IPU video transform

I added the library libfslcodec.

I try to play a video with aac or mp3 sound. The video is OK, but there is no sound. I suspect that the libfslcodec is not installed. If I added other codecs, it works fine. In all cases (with and without extra codecs), I have a warning, that there is no codec for this audio format

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

2,017 Views
igorpadykov
NXP Employee
NXP Employee

Hi   Taverdet

these plugins are part of gstreamer-imx plugins developed and supported by community.
Note there are also nxp plugins used in official nxp bsps described on link
http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....
Difference between two plugins are described on: trac.gateworks.com/wiki/Yocto/gstreamer
Issues with gstreamer-imx plugins may be posted on meta-fsl-arm mailing list, so
that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Alternatively one can use nxp gstreamer plugins, please follow guidelines provided in nxp linux doc package
https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply