How to initialize i.MX 8QuadMax?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to initialize i.MX 8QuadMax?

2,579 Views
aviau
Contributor II

Hello,

I am not able to initialize the i.MX 8QuadMax card, when I connect it to the computer (windows 10) nothing happens, when I try to access it through the terminal also do not get results, we have somewhere to download the bootloader file ??

0 Kudos
Reply
3 Replies

2,388 Views
pawans
Contributor I

Getting this error

 

This script is validated with uuu 1.2.91 version, please align with this version.
dtbo is supported
dual slot is supported
generate lines to flash partition-table-13GB.img to the partition of gpt
generate lines to flash u-boot-imx8mm.imx to the partition of bootloader0
generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a
generate lines to flash dtbo-imx8mm.img to the partition of dtbo_b
generate lines to flash boot.img to the partition of boot_b
generate lines to flash system.img to the partition of system_b
generate lines to flash vendor.img to the partition of vendor_b
generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_b
uuu script generated, start to invoke uuu with the generated uuu script
./uuu_imx_android_flash.sh: line 524: uuu: command not found
root@chetuiwk2066:/home/chetu/TechNexionNew/out/target/product/pico_imx8mm#

0 Kudos
Reply

2,423 Views
aviau
Contributor II

This script is validated with uuu 1.2.91 version, please align with this version.
dual bootloader is supported
dtbo is supported
dual slot is supported
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash spl-imx8mq.bin to the partition of bootloader0
generate lines to flash bootloader-imx8mq.img to the partition of bootloader_a
generate lines to flash dtbo-imx8mq.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash vbmeta-imx8mq.img to the partition of vbmeta_a
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.89-0-gd7d8504

Wait for Known USB Device Appear...
Error: fail open file: >u-boot-imx8mq-evk-uuu.imx.link

0 Kudos
Reply

2,423 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anderson

what "card" used in the case. If this is NXP i.MX8QM MEK reference board

one can follow documentation on
i.MX Software | NXP 

If this is custom board you can try to get documentation and tools through

NXP local marketing office.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply