How to implement zigbee driver in sabre sd imx6q board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to implement zigbee driver in sabre sd imx6q board?

1,898件の閲覧回数
divyardharan
Contributor III

Hi,

We need to implement zigbee driver in sabre sd imx6q board.We are using telegesis development kit Model ETRX357.The BSP is timesys linux.Kindly help with sujjestions.

Thanks in Advance,

Divya

0 件の賞賛
返信
2 返答(返信)

1,678件の閲覧回数
timesyssupport
Senior Contributor II

Hello,

We are not in posession of that evaluation hardware, and it seems the drivers for this module are not public. As such, we are not able to directly assist with this issue. Please file a request in our Support system divyardharan so that we can discuss how to assist in integrating this third party hardware. Please also include a description of the kernel version you are running when filing the request.

Thank you,

Timesys Support

0 件の賞賛
返信

1,678件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

timesyssupport, do you have any comment for this request?

0 件の賞賛
返信