How to get gcc source code for i.MX6 Linux BSP.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get gcc source code for i.MX6 Linux BSP.

ソリューションへジャンプ
4,357件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 Linux BSP (L3.0.35_4.1.0 & L3.10.17_1.0.2-ga).

I'm looking for the source code of GCC compiler.

I found the source code for i.MX51 in the following URL.

i.MX51 Evaluation Kit|Freescale

Is GCC compiler source code for i.MX6 opened same as the one for i.MX51 even though I cannot found it on i.MX6 web page?

Or should I download it from Linaro web site?

Best Regards,

Satoshi Shimoda

タグ(1)
0 件の賞賛
返信
1 解決策
3,680件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

!!Hi Satoshi

please look at attached documents for compilers selection.

Source codes can be found on gcc web site

GCC, the GNU Compiler Collection- GNU Project - Free Software Foundation (FSF)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,681件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

!!Hi Satoshi

please look at attached documents for compilers selection.

Source codes can be found on gcc web site

GCC, the GNU Compiler Collection- GNU Project - Free Software Foundation (FSF)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信