How to get camera RAW data in i.MX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get camera RAW data in i.MX8

885 Views
xu_ji1
Contributor V

Hello,

I used max9286 and camera is mono Raw 12bit output and max9286 also use Raw12 output to CSI,

How can I get the Raw data max9286 output?

I used application get camera data set format V4L2_PIX_FMT_Y16,why it happened VIDIOC_S_FMT failed?

does i.MX8 not support this format?

Thanks

2 Replies

741 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xu

yes ISI supports that format, unfortunately linux software seems not support yet.

For help one can apply to Commercial Support and Engineering Services | NXP 

or try to convert to other formats using Soft ISP :

https://www.nxp.com/docs/en/application-note/AN12060.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

741 Views
xu_ji1
Contributor V

Hi,

And how can I dump camera Raw data?

Thanks

0 Kudos
Reply