I had IMX25 PDK board and want to boot it up.
I follow AN12024 to try to build it on my PC but failed, linkage http://commondatastorage.googleapis.com/git-repo-downloads/repo can not be accessed.
I try to use latest Yocto use guide to build it. and seem that Yocto project don't support IMX25 PDK board. Is this right? How can I build image for the board?
healy@healy-virtual-machine:~/fsl-release-bsp/sources/meta-fsl-arm/conf/machine$ ls
imx23evk.conf imx6slllpddr2arm2.conf imx6ulevk.conf
imx28evk.conf imx6slllpddr3arm2.conf imx6ull14x14ddr3arm2.conf
imx51evk.conf imx6solosabreauto.conf imx6ull14x14evk.conf
imx53ard.conf imx6solosabresd.conf imx6ull9x9evk.conf
imx53qsb.conf imx6sx14x14arm2.conf imx7d12x12ddr3arm2.conf
imx6dlsabreauto.conf imx6sx17x17arm2.conf imx7d12x12lpddr3arm2.conf
imx6dlsabresd.conf imx6sx19x19ddr3arm2.conf imx7d19x19ddr3arm2.conf
imx6qdlsolo.conf imx6sx19x19lpddr2arm2.conf imx7d19x19lpddr2arm2.conf
imx6qpsabreauto.conf imx6sx_all.conf imx7d19x19lpddr3arm2.conf
imx6qpsabresd.conf imx6sxsabreauto.conf imx7dsabresd.conf
imx6qsabreauto.conf imx6sxsabresd.conf include
imx6qsabresd.conf imx6ul14x14ddr3arm2.conf ls1021atwr.conf
imx6slevk.conf imx6ul14x14lpddr2arm2.conf twr-vf65gs10.conf
imx6sll_all.conf imx6ul7d.conf
imx6sllevk.conf imx6ul9x9evk.conf
healy@healy-virtual-machine:~/fsl-release-bsp/sources/meta-fsl-arm-extra/conf/machine$ ls
apalis-imx6.conf imx233-olinuxino-maxi.conf nitrogen6sx.conf
cfa10036.conf imx233-olinuxino-micro.conf nitrogen6x.conf
cfa10037.conf imx233-olinuxino-mini.conf nitrogen6x-lite.conf
cfa10049.conf imx233-olinuxino-nano.conf nitrogen7.conf
cfa10055.conf imx6dl-riotboard.conf pcm052.conf
cfa10056.conf imx6qdl-variscite-som.conf tx6q-10x0.conf
cfa10057.conf imx6q-dms-ba16.conf tx6q-11x0.conf
cfa10058.conf imx6qsabrelite.conf tx6s-8034.conf
cgtqmx6.conf imx6sl-warp.conf tx6s-8035.conf
cm-fx6.conf imx6ul-pico-hobbit.conf tx6u-8033.conf
colibri-imx6.conf imx7s-warp.conf tx6u-80x0.conf
colibri-imx7.conf include tx6u-81x0.conf
colibri-vf.conf m28evk.conf ventana.conf
cubox-i.conf m53evk.conf wandboard.conf
Hello Healy Sun,
There is support for the i.MX25 PDK but only as part of the Community BSP, which is an open source project supported and maintained by the community and part of the Yocto Project.
You can find more details on this on the following link:
https://freescale.github.io/
The latest official BSP release for the i.MX25 was released before Yocto so there are no official Yocto BSP Releases for this processor.
My apologies for the inconvenience.
Regards,
got it
I would like to try it
Thank you so much!