How to get a display to work on i.MX53 Quick Start Board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get a display to work on i.MX53 Quick Start Board?

1,099 Views
LuanLe
Contributor I

Hello,

 

I am first time here so I don't know if I am in the right place.  I am evaluating the i.MX53 processor and need some help with the i.MX53 QSB.   I have problem getting the display to work.  Below are what I did

 

- Flashed a SD card with a WinEC 7 image (eboot.nb0 and nk.nb0) with my XP.  The image was downloaded from Adeneo for the LVDS display build.

- Plugged the SD card into the socket on the QSB

- Connected an external monitor to the board through a DVI-to-HDMI adaptor (  also tried the VGA connector without success)

- Power up the device and saw lots of LED on the board go on

 

but got a dark display.  I am not sure if I flashed the right build for the hardware or I need some special display.

Please tell me if I am missing anything.

 

Thanks,

Luan

0 Kudos
Reply
1 Reply

948 Views
c0170
Senior Contributor III

Hi LuanLe,

 

you should post this question to the i.MX section but that one is read-only, therefore visit this webpage:

i.MX section on freescale.com

 

You might find faster the help you need. This section is dedicated to MQX RTOS.

 

Regards,

MartinK

 

0 Kudos
Reply