How to enable rtmp plugins in gstreamer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable rtmp plugins in gstreamer

4,489件の閲覧回数
fulinux
Contributor IV

Hi,

   HW: imx6qsabresd + usb web camera

   SW:yocto+L4.1.15_2.1.0

  i want to use my usb web camera to become a live source, and push camera video streaming with rtmp protocal.

 I find gstreamer dose not enable rtmp when i use gstreamer tool gst-launch-1.0. look at this:

[fulinux@dev-ubuntu build-wayland-4.1.15_2.1.0]$ cat tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/gstreamer1.0-plugins-bad/1.8.1-r0/build/config.log  | less
This file contains any messages produced by compilers while
running configure, to aid debugging if configure makes a mistake.

It was created by GStreamer Bad Plug-ins configure 1.8.1, which was
generated by GNU Autoconf 2.69.  Invocation command line was

  $ ../gst-plugins-bad-1.8.1/configure --build=x86_64-linux --host=arm-poky-linux-gnueabi --target=arm-poky-linux-gnueabi --prefix=/usr --exec_prefix=/usr --bindir=/usr/bin --sbindir=/usr/sbin --libexecdir=/usr/libexec --datadir=/usr/share --sysconfdir=/etc --sharedstatedir=/com --localstatedir=/var --libdir=/usr/lib --includedir=/usr/include --oldincludedir=/usr/include --infodir=/usr/share/info --mandir=/usr/share/man --disable-silent-rules --disable-dependency-tracking --with-libtool-sysroot=/home/fulinux/fsl-release-bsp/build-wayland-4.1.15_2.1.0/tmp/sysroots/imx6qsabresd --enable-introspection --disable-examples --enable-decklink --enable-dvb --enable-fbdev --enable-shm --enable-vcd --disable-acm --disable-android_media --disable-apexsink --disable-apple_media --disable-avc --disable-bs2b --disable-chromaprint --disable-cocoa --disable-daala --disable-dc1394 --disable-direct3d --disable-directsound --disable-dts --disable-gme --disable-gsm --disable-kate --disable-ladspa --disable-libde265 --disable-libvisual --disable-linsys --disable-lv2 --disable-mimic --disable-mpeg2enc --disable-mplex --disable-musepack --disable-nas --disable-ofa --disable-openexr --disable-openh264 --disable-openjpeg --disable-openni2 --disable-opensles --disable-pvr --disable-qt --disable-sdl --disable-sdltest --disable-sndio --disable-soundtouch --disable-spandsp --disable-spc --disable-teletextdec --disable-timidity --disable-vdpau --disable-wasapi --disable-wildmidi --disable-wininet --disable-winks --disable-winscreencap --disable-x265 --disable-xvid --disable-zbar --enable-nls --disable-assrender --enable-bluez --enable-bz2 --enable-curl --enable-dash --disable-debug --disable-directfb --enable-dtls --disable-faac --disable-faad --disable-flite --disable-fluidsynth --enable-gles2 --enable-egl --disable-gtk3 --enable-hls --disable-libmms --disable-libssh2 --disable-modplug --enable-neon --disable-openal --enable-opencv --disable-opengl --disable-opus --enable-orc --disable-resindvd --enable-rsvg --disable-rtmp --enable-sbc --disable-schro --enable-smoothstreaming --enable-sndfile --disable-srtp --enable-uvch264 --disable-valgrind --disable-voaacenc --disable-voamrwbenc --enable-wayland --disable-x11 --enable-webp

1、How can i enable rtmp in gst-plugins-bad?

2、How can I push video and audio streaming to rtmp? can you give me some support?

3、I Have used nginx make a RTMP server in ubuntu, and i use gst-launch-1.0 to pull rtmp streaming, like this:

gst-launch-1.0 playbin uri=rtmp://xxxxxx/live/test

it works well sometimes, but not most of the time.  it has the same phenomenon in BSP3.0.35_4.1.0 with gsreamer-0.10. Can you give me some help?

my english is so poor 0.0

thank you!

fulinux.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,659件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi fulinux

as this is special gstreamer issue one can post it on dedicated gstreamer forums,

so more people could try to assist you

GStreamer: Mailing Lists 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,659件の閲覧回数
fulinux
Contributor IV

HI igorpadykov,

    Thank you for you reply!

    I'm new, i don't know how to enable rtmp in yocto, and i don't know how to search my question in GStreamer: Mailing Lists.

    thanks.

fulinux.

0 件の賞賛
返信