How to enable LAN9500?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable LAN9500?

4,105 Views
mingmingyuan
Contributor III

我们的硬件设计采用的是LAN9500来扩展网口的,请问如何enableLAN9500?

0 Kudos
Reply
4 Replies

3,414 Views
igorpadykov
NXP Employee
NXP Employee

Hi mingming

it is necessary to add to linux lan9500 driver,

seems it was tested below

USB to Ethernet adapter - ArmadeusWiki

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,414 Views
mingmingyuan
Contributor III

在enable LAN9500的时候,make linux-menuconfig是报错的,只能执行make menuconfig

ymm@ymm-VirtualBox:~/ltib/rpm/BUILD/linux$ make linux-menuconfig

make[1]: *** 没有规则可以创建目标“linux-menuconfig”。 停止。

make: *** [linux-menuconfig] 错误 2

ymm@ymm-VirtualBox:~/ltib/rpm/BUILD/linux$

0 Kudos
Reply

3,414 Views
mingmingyuan
Contributor III

dear sir:

感谢您的支持和帮助!

我已经把LAN9500的driver跑起来了,log里看到如下信息

smsc95xx 2-1:1.0: eth1: register 'smsc95xx' at usb-fsl-ehci.1-1, smsc95xx USB 2.0 Ethernet, 0e:0c:c5:19:54:6c

但是我执行ifconfig命令,没有查看到任何网络端口啊,我理解应该会有eth1这个网络端口

0 Kudos
Reply

3,414 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply