How to enable HDMI Input in kernel for i.mx8QMax

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable HDMI Input in kernel for i.mx8QMax

2,850件の閲覧回数
santhosh2
Contributor IV

Hi,

 I want to connect the Camera to HDMI Input and test the video stream, so how to  enable HDMI Input in kernel in i.mx8QMax.

Regards

Santhosh Kumar S

0 件の賞賛
返信
3 返答(返信)

2,741件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

currently this feature is not supported, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,740件の閲覧回数
santhosh2
Contributor IV

NXP Bangalore Team Confirmed that this feature is supported.

Attached the page

0 件の賞賛
返信

2,740件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

this image is general description.

Note this part is not publicly released yet and linux does not support

all its functionality.

Best regards
igor

0 件の賞賛
返信