How to enable HDMI Input in kernel for i.mx8QMax and how to test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable HDMI Input in kernel for i.mx8QMax and how to test

1,408 Views
santhosh2
Contributor IV

Hi,

I have the HDMI camera and i  would like to take HDMI camera input and display on the lcd, How to enable HDMI Input in kernel for i.mx8QMax and how to test

0 Kudos
Reply
3 Replies

1,241 Views
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

in general one can try using fsl-imx8qm-mek-hdmi-in.dts

V4l2 video device  ‘/dev/videox’ and command
/unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 0

imx-test - i.MX Driver Test Application Software 

but this functionality is still under development.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,241 Views
santhosh2
Contributor IV

Hi,

I have tested but it didnt work. Can you please let me know any document or procedure is there

Regards

Santhosh

0 Kudos
Reply

1,241 Views
igorpadykov
NXP Employee
NXP Employee

it is not supported according to latest documentation

i.MX Software | NXP 

~igor

0 Kudos
Reply