How to display monitor via USB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to display monitor via USB

1,770 次查看
wangvictor
Contributor III

Hi All,

I'm using i.MX6 sabresd  DL for my cpu and linux kernel driver for version 4.1.15.

I'm trying to display the monitor via USB.

Which driver I should open and build in?

And what else I have to do ?

Thanks in Advance!

标记 (3)
0 项奖励
回复
2 回复数

1,597 次查看
igorpadykov
NXP Employee
NXP Employee

Hi victor

seems one needs to implement support for usb monitor driver described on

http://www.usb.org/developers/docs/devclass_docs/usbmon10.pdf 

Chapter 39 CHIPIDEA USB Driver attached Linux Manual describes

current lnux usb driver capabilities.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,597 次查看
wangvictor
Contributor III

Is this just can support X86 structure CPU ?

Or I can using on the ARM structure?

0 项奖励
回复