How to disable level 2 cache on a IMX6UL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to disable level 2 cache on a IMX6UL?

2,260件の閲覧回数
CarstenBode
Contributor II

Hello,

I want to test my application that should run finally on a IMX6G0 ( with no L2C) on the EVK board that uses a IMX6G2 ( with 128K L2C). For testing I would like to disable the L2C on the IMX6G2, but I didn´t find where.

Any idea how to disable L2C and keep L1C still enabled?

Best regards

Carsten Bode

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,056件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Carsten

seems this is not possible according to answer on arm communty

https://community.arm.com/thread/9723

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,056件の閲覧回数
CarstenBode
Contributor II

Hi Igor,

I want to test if th IMX6G0 is fast enough for my application.

So I need a evalboard with the IMX6G0.

Best regards

Carsten

0 件の賞賛
返信