How to disable USB3.0 and force USB3.0 to USB2.0 in kernel config for maaxboard and maaxboard-mini?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to disable USB3.0 and force USB3.0 to USB2.0 in kernel config for maaxboard and maaxboard-mini?

ソリューションへジャンプ
2,295件の閲覧回数
gonewithwind-peter
Senior Contributor I

hi all

I use maaxboard and maaxboard-mini board, we need to connect a USB disk(2.0 and 3.0),

but after insert USB3.0 disk, there is an error  ,  someone posted before here and need to update the kernel :https://community.nxp.com/t5/i-MX-Processors/USB3-0-disconnect-periodic-on-i-mx8mq/m-p/1155828/highl...

I do not want change to new yocto branch(too much work,  our node code not work...).

can I and how to disable USB3.0 and force USB3.0 to USB2.0 in kernel config?

 

Thank you very much.

0 件の賞賛
返信
1 解決策
2,287件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Peter

 

unfortunately there is no software way to disable USB3.0.

i.MX8M Mini has not USB3.0.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,282件の閲覧回数
gonewithwind-peter
Senior Contributor I

@igorpadykov 

thanks. got it

0 件の賞賛
返信
2,288件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Peter

 

unfortunately there is no software way to disable USB3.0.

i.MX8M Mini has not USB3.0.

 

Best regards
igor

0 件の賞賛
返信