How to debug deadlock on IMX6Q?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to debug deadlock on IMX6Q?

1,491件の閲覧回数
kris_fei
Contributor III

I am porting Android Lollipop 5.1,  it stuck at bootanimation, and reset after a while whose reboot reason is watchdog.

It seems there's a deadlock, how do i debug?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,412件の閲覧回数
b36401
NXP Employee
NXP Employee

First please make sure that you set right options in u-boot configuration.

You can refer "Boot-up configurations" chapter of Android User's Guide.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,412件の閲覧回数
kris_fei
Contributor III

Sorry, maybe i didn't describe clearly. I mean the system boots up to android bootanimation, which just displays "ANDROID" fonts,

then it hang up and reboot.

0 件の賞賛
返信