How to customize kernel for IMX6UL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to customize kernel for IMX6UL?

1,402 Views
paolosantini
Contributor III

I'm trying to customize Linux Kernel for a Variscite DART 6UL  (my aim is to use a 7" TFT display and I'd like to activate hsync and vsync). Following a tutorial written by Variscite to customize a display, I modified a .dtsi file, but at the end of the Kernel compilation procedure, I didn't find a solution to my problem.

Someone can help me?

0 Kudos
Reply
1 Reply

1,271 Views
igorpadykov
NXP Employee
NXP Employee

Hi Paolo

one can look at nxp documentation:

Task #10 - How to create a custom layer 

i.MX Yocto Project: How can I (quickly) modify the kernel and test it? 

specific isues with third party releases are supported by vendors of these software.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply