How to customize kernel for IMX6UL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to customize kernel for IMX6UL?

1,406件の閲覧回数
paolosantini
Contributor III

I'm trying to customize Linux Kernel for a Variscite DART 6UL  (my aim is to use a 7" TFT display and I'd like to activate hsync and vsync). Following a tutorial written by Variscite to customize a display, I modified a .dtsi file, but at the end of the Kernel compilation procedure, I didn't find a solution to my problem.

Someone can help me?

0 件の賞賛
返信
1 返信

1,275件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Paolo

one can look at nxp documentation:

Task #10 - How to create a custom layer 

i.MX Yocto Project: How can I (quickly) modify the kernel and test it? 

specific isues with third party releases are supported by vendors of these software.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信