How to create mipi panel enabled OTA package on IMX8Mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to create mipi panel enabled OTA package on IMX8Mini

1,594件の閲覧回数
13614278
Contributor III

I had IMX8Mini EVK, which has MIPI panel., and I am using Android9

By default, the Android build image is HDMI, that's why every time I flash the EVK, I had to use -d mipi:

./uuu_imx_android_flash.sh -f imx8mm -a -e -d mipi

to let my MIPI screen up.

Unfortunately, when I create the OTA package(make otapackage), it seems it still use HDMI by default, so when I OTA the EVK, the screen didn't UP.

Could someone help me to let me know HOWTO create a MIPI-default OTA package instead of HDIM?

Thanks a lot.

0 件の賞賛
返信
1 返信

1,473件の閲覧回数
shivanipatel
Senior Contributor II

Hi, Yang Songxiang 

You need to specify the mipi dtbo image to the "BOARD_PREBUILT_DTBOIMAGE" variable for MIPI panel display in OTA package.

e.g BOARD_PREBUILT_DTBOIMAGE := out/target/product/evk_8mm/dtbo-imx8mm-mipi-panel.img

This variable is defined in the BoardConfig.mk file which resides in Android Source at "${MY_ANDROID}/device/fsl/imx8m/evk_8mm/BoardConfig.mk".

After this, you can generate the OTA package for evk_8mm with MIPI panel display.

Hope this will help you.

Let us know in case of any concern.

Regards,

Shivani

0 件の賞賛
返信