Dear NXP ,
HW : srg_imx8mplus
SW : 5.10.9-1.0.0
I run command in imx8mplus plarform as follows:
echo "host" >> /sys/kernel/debug/usb/38200000.dwc3/mode
/unit_tests/memtool -32 0x38200430=0x0A010340
It can output USB 3.0 eye diagram because there is no USB HUB on imx8mplus platform.
I run the same command on the srg_imx8mplus platform but it didn't output USB 3.0 eye diagram.
I asked the USB HUB FAE and he told me . NXP imx8mplus must run command to USB HUB:
USB HUB port1,port2,port3,port4
May you tell me how to run the command (USB HUB port)
srg_imx8mplus HW: