How to configure the I.MX 28 LCD Interface change RGB to BT601

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure the I.MX 28 LCD Interface change RGB to BT601

1,321件の閲覧回数
rjagan_mca
Contributor I

Hi

i have Tianma's MT035 LCD module 3.5" display. This display device can be programmable to RGB mode or CCIR Mode.

so i successfully configure this 3.5" display from rgb mode to bt601 mode by using spi communication.

in imx28 datasheet, the lcd interface describes it will be converted to RGB / BT601 / BT656 or anyone (Defaulty it's outputs RGB 8 bit)

Now what i want is,

How can i configure the Display pins to output BT601 Format?

Best Regards

Jagan


ラベル(4)
0 件の賞賛
返信
1 返信

765件の閲覧回数
Yuri
NXP Employee
NXP Employee

Generally section 33.2.9 “ITU-R BT.656 Digital Video Interface (DVI)”
of the i.MX28 Reference Manual provides information about BT.656 using :

“ITU-R BT.656 Digital Video Interface shown below transmits 4:2:2 YCbCr digital

component video to a digital video encoder that can translate it into 525/60 or 625/50

analog TV signal. Unique timing codes (timing reference signals) are embedded within

the video stream to indicate the different timing events that would have been otherwise

indicated by VSYNC, HSYNC and BLANK signals. The hardware supports 8-bit data

transfers; the pins are shared with the lower 8 bits of LCD data bus. The LCD_RS pin is

shared with the clock signal of the interface (called CCIRCLK here for uniqueness).

CCIRCLK also can be obtained on the LCD_DOTCK pin. The mode shares the write

FIFO with the LCD interface and the associated pipeline. The programmable parameters

in registers HW_LCDIF_DVICTRL0-3 allow setting the total number of horizontal lines

per frame, vertical and horizontal blanking interval, odd and even field start and end

positions, and so on. In short, these parameters are provided to ensure that the hardware

has enough flexibility to generate the right 525/60 or 625/50 data streams. Most of the

initialization steps in Initializing the LCDIF such as data shifting, swizzle, and so on, are

applicable to DVI mode also. The register descriptions in the programmable registers

section at the end of this chapter include example code for programming the

DVICTRL0-3 registers.

In DVI mode, HW_LCDIF_CTRL_BYPASS_COUNT bit must be set to 1. To end the

current transfer, the software should make the DVI_MODE bit the value 0, so that all

data that is currently in the LCDIF LFIFO and TXFIFO is transmitted. Once that transfer

is complete, the block will automatically clear the RUN bit and assert the

cur_frame_done interrupt.”

So, please take a look at the examples in following sections of the i.MX28 Reference Manual :

- 33.4.13 “Digital Video Interface Control0 Register (HW_LCDIF_DVICTRL0)”

- 33.4.14 “Digital Video Interface Control1 Register (HW_LCDIF_DVICTRL1)”

- 33.4.15 “Digital Video Interface Control2 Register (HW_LCDIF_DVICTRL2)”

- 33.4.16 “Digital Video Interface Control3 Register (HW_LCDIF_DVICTRL3)”

- 33.4.17 “Digital Video Interface Control4 Register (HW_LCDIF_DVICTRL4)”

For general LCDIF initialization please refer to the OBDS package

< https://www.freescale.com/webapp/Download?colCode=IMX_OBDS&appType=license&location=null >

< http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX280&nodeId=018rH3ZrDRA24A&fpsp=1&... >

0 件の賞賛
返信