How to config SDIO3.0 IMX6qp Android P

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to config SDIO3.0 IMX6qp Android P

1,525件の閲覧回数
jianhua_zhuang
Contributor I

How to config SDIO3.0 IMX6qp imx-p9.0.0_2.2.0

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 返信

1,448件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jianhua.zhuang

for SDIO3.0 there are no special configs, only appropriate driver

(if for example this is wifi card), however board should have voltage switch

described as "UHS-1 I/O logic level change" on p.6 i.MX6Q Sabre AI board

schematic SCH-27142

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------