How to config SDIO3.0 IMX6qp Android P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to config SDIO3.0 IMX6qp Android P

1,565 Views
jianhua_zhuang
Contributor I

How to config SDIO3.0 IMX6qp imx-p9.0.0_2.2.0

Labels (3)
0 Kudos
Reply
1 Reply

1,488 Views
igorpadykov
NXP Employee
NXP Employee

Hi jianhua.zhuang

for SDIO3.0 there are no special configs, only appropriate driver

(if for example this is wifi card), however board should have voltage switch

described as "UHS-1 I/O logic level change" on p.6 i.MX6Q Sabre AI board

schematic SCH-27142

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------