How to compile totem-3.0.1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to compile totem-3.0.1?

1,644 Views
franklee19731
Contributor I

Out project is based on iMX6 Dual core and Ubuntu,  I have tested that the totem media player is very powerful and very suit for us except that we may do some customization for UI.

But after I did ./configure in the totem-3.0.1 source code directory,   it complained that several packages were need for the build. I tried to search gtk+3.0 with "apt-cache search" command, but there is no result.

I want to ask how to configure and build totem 3.0.1, and if Freescale did some modifications on the source code of totem-3.0.1.

Below is the  configuration log. And I also upload the totem 3.0.1 source code in the attachment.

=====================================================================================

checking whether to enable maintainer-specific portions of Makefiles... no

checking for a BSD-compatible install... /usr/bin/install -c

checking whether build environment is sane... yes

checking for a thread-safe mkdir -p... /bin/mkdir -p

checking for gawk... no

checking for mawk... mawk

checking whether make sets $(MAKE)... yes

checking whether NLS is requested... yes

checking for style of include used by make... GNU

checking for gcc... gcc

checking whether the C compiler works... yes

checking for C compiler default output file name... a.out

checking for suffix of executables...

checking whether we are cross compiling... no

checking for suffix of object files... o

checking whether we are using the GNU C compiler... yes

checking whether gcc accepts -g... yes

checking for gcc option to accept ISO C89... none needed

checking dependency style of gcc... gcc3

checking for intltool >= 0.40.0... 0.50.2 found

checking for intltool-update... /usr/bin/intltool-update

checking for intltool-merge... /usr/bin/intltool-merge

checking for intltool-extract... /usr/bin/intltool-extract

checking for xgettext... /usr/bin/xgettext

checking for msgmerge... /usr/bin/msgmerge

checking for msgfmt... /usr/bin/msgfmt

checking for gmsgfmt... /usr/bin/msgfmt

checking for perl... /usr/bin/perl

checking for perl >= 5.8.1... 5.14.2

checking for XML::Parser... ok

checking whether ln -s works... yes

checking for pkg-config... /usr/bin/pkg-config

checking pkg-config is at least version 0.9.0... yes

checking gnome-doc-utils >= 0.20.3... yes

checking for gobject-introspection... no

checking for g++... g++

checking whether we are using the GNU C++ compiler... yes

checking whether g++ accepts -g... yes

checking dependency style of g++... gcc3

checking whether gcc and cc understand -c and -o together... yes

checking build system type... armv7l-unknown-linux-gnueabi

checking host system type... armv7l-unknown-linux-gnueabi

checking how to print strings... printf

checking for a sed that does not truncate output... /bin/sed

checking for grep that handles long lines and -e... /bin/grep

checking for egrep... /bin/grep -E

checking for fgrep... /bin/grep -F

checking for ld used by gcc... /usr/bin/ld

checking if the linker (/usr/bin/ld) is GNU ld... yes

checking for BSD- or MS-compatible name lister (nm)... /usr/bin/nm -B

checking the name lister (/usr/bin/nm -B) interface... BSD nm

checking the maximum length of command line arguments... 1572864

checking whether the shell understands some XSI constructs... yes

checking whether the shell understands "+="... yes

checking how to convert armv7l-unknown-linux-gnueabi file names to armv7l-unknown-linux-gnueabi format... func_convert_file_noop

checking how to convert armv7l-unknown-linux-gnueabi file names to toolchain format... func_convert_file_noop

checking for /usr/bin/ld option to reload object files... -r

checking for objdump... objdump

checking how to recognize dependent libraries... pass_all

checking for dlltool... no

checking how to associate runtime and link libraries... printf %s\n

checking for ar... ar

checking for archiver @FILE support... @

checking for strip... strip

checking for ranlib... ranlib

checking command to parse /usr/bin/nm -B output from gcc object... ok

checking for sysroot... no

checking for mt... mt

checking if mt is a manifest tool... no

checking how to run the C preprocessor... gcc -E

checking for ANSI C header files... yes

checking for sys/types.h... yes

checking for sys/stat.h... yes

checking for stdlib.h... yes

checking for string.h... yes

checking for memory.h... yes

checking for strings.h... yes

checking for inttypes.h... yes

checking for stdint.h... yes

checking for unistd.h... yes

checking for dlfcn.h... yes

checking for objdir... .libs

checking if gcc supports -fno-rtti -fno-exceptions... no

checking for gcc option to produce PIC... -fPIC -DPIC

checking if gcc PIC flag -fPIC -DPIC works... yes

checking if gcc static flag -static works... yes

checking if gcc supports -c -o file.o... yes

checking if gcc supports -c -o file.o... (cached) yes

checking whether the gcc linker (/usr/bin/ld) supports shared libraries... yes

checking whether -lc should be explicitly linked in... no

checking dynamic linker characteristics... GNU/Linux ld.so

checking how to hardcode library paths into programs... immediate

checking whether stripping libraries is possible... yes

checking if libtool supports shared libraries... yes

checking whether to build shared libraries... yes

checking whether to build static libraries... yes

checking how to run the C++ preprocessor... g++ -E

checking for ld used by g++... /usr/bin/ld

checking if the linker (/usr/bin/ld) is GNU ld... yes

checking whether the g++ linker (/usr/bin/ld) supports shared libraries... yes

checking for g++ option to produce PIC... -fPIC -DPIC

checking if g++ PIC flag -fPIC -DPIC works... yes

checking if g++ static flag -static works... yes

checking if g++ supports -c -o file.o... yes

checking if g++ supports -c -o file.o... (cached) yes

checking whether the g++ linker (/usr/bin/ld) supports shared libraries... yes

checking dynamic linker characteristics... (cached) GNU/Linux ld.so

checking how to hardcode library paths into programs... immediate

configure: creating ./config.lt

config.lt: creating libtool

checking for pkg-config... (cached) /usr/bin/pkg-config

checking pkg-config is at least version 0.9.0... yes

checking for glib-genmarshal... /usr/bin/glib-genmarshal

checking for glib-mkenums... /usr/bin/glib-mkenums

checking whether to enable easy codec installation support... auto

checking for MISSING_PLUGINS... yes

checking for GST... yes

checking GStreamer 0.10 inspection tool... yes

checking GStreamer 0.10 playbin2 plugin... yes

checking GStreamer 0.10 ffmpegcolorspace plugin... yes

checking GStreamer 0.10 videoscale plugin... yes

checking GStreamer 0.10 gconfaudiosink plugin... yes

checking GStreamer 0.10 gconfvideosink plugin... yes

checking GStreamer 0.10 goom plugin... yes

checking which smclient backend to use... no

checking for DEPENDENCY... no

configure: error: Package requirements (

  glib-2.0 >= 2.27.92

  gio-2.0 >= 2.27.92

  gtk+-3.0 >= 2.99.3

  gdk-x11-3.0 >= 2.99.3

  gmodule-2.0

  totem-plparser >= 2.32.4

  gstreamer-tag-0.10 >= 0.10.26

  cairo) were not met:

No package 'gtk+-3.0' found

No package 'gdk-x11-3.0' found

No package 'totem-plparser' found

Consider adjusting the PKG_CONFIG_PATH environment variable if you

installed software in a non-standard prefix.

Alternatively, you may set the environment variables DEPENDENCY_CFLAGS

and DEPENDENCY_LIBS to avoid the need to call pkg-config.

See the pkg-config man page for more details.

Original Attachment has been moved to: totem_3.0.1.orig.tar.gz

Labels (4)
0 Kudos
Reply
1 Reply

1,150 Views
jack_mao
NXP Employee
NXP Employee

Hi Frank,

       The totem is opensource code, not in our support range, you could find solution for your issue in the internet

best regards

Jack

0 Kudos
Reply