How to change system partition size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change system partition size

2,679件の閲覧回数
rajucm
Contributor III

Hi All,

I am using Android 4.4.2

I need change system partition size to 512 MB.

Currently it is showing 354MB. Please help me to change system partition size.

root@sabresd_6dq:/ # df

Filesystem               Size     Used     Free   Blksize

/dev                   913.6M   136.0K   913.5M   4096

/sys/fs/cgroup         913.6M    12.0K   913.6M   4096

/mnt/secure            913.6M     0.0K   913.6M   4096

/mnt/asec              913.6M     0.0K   913.6M   4096

/mnt/obb               913.6M     0.0K   913.6M   4096

/mnt/shm              1024.0K     0.0K  1024.0K   4096

/system                354.3M   222.7M   131.6M   4096

/data                   13.1G   199.6M    12.9G   4096

/cache                 495.8M    10.3M   485.6M   1024

/device                  7.7M     1.0M     6.7M   1024

/mnt/shell/emulated     13.1G   199.6M    12.9G   4096

root@sabresd_6dq:/ #

Thanks,

Raju

ラベル(4)
0 件の賞賛
返信
1 返信

2,387件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Raju CM,

You can refer to the 4.1.1 Storage partitions in Android_User's_Guide.pdf .
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信