How to capture crash log using kdump

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to capture crash log using kdump

6,199 Views
Raana
Contributor III

Dear Team,

Right now, I'm using i.Mx8x based custom board.

BSP version is, imx-yocto-L4.14.98_2.0.0_ga

There I'm trying to capture the crash log of my standard kernel if any panic occurs.

I'm using 'kdump' for the same. I'm following below procedure to achieve kdump.

1) Precondition (Kernel)

There are two kernels,
- Standard (production) kernel - kernel we normally boot
- Crash (capture) kernel - kernel specially used for collecting crash dumps

a) Kernel configuration for Standard kernel
CONFIG_KEXEC=y
CONFIG_SYSFS=y
CONFIG_DEBUG_INFO=Y

b) Kernel configuration for capture kernel
CONFIG_CRASH_DUMP=y
CONFIG_PROC_VMCORE=y
(CONFIG_PROC_VMCORE is set by default when CONFIG_CRASH_DUMP is selected.)

NOTE: Keep both a kernel (Image and *.bin) in /boot directory

2) Precondition (kexec)
Install the "kexec-tools" in Yocto.

3) Boot the Standard kernel with boot parameter "crashkernel"
-> setenv bootargs 'crashkernel=256M'

4) Load the capture kernel with following command
kexec -p /boot/Image --command-line="root=/dev/mmcblk0p2 console=ttyLP0,115200 earlycon=lpuart32,0x5a060000,115200 rootwait rootfstype=ext4 ro 1 maxcpus=1 reset_devices"

5) To test,
echo 1 > /proc/sys/kernel/sysrq
echo c > /proc/sysrq-trigger

But my capture kernel is not booting properly. This also getting crashed in-between.

Is my above procedure correct?

Thank You.

Best Regards,

J.P.Raja

0 Kudos
Reply
1 Reply

6,139 Views
b36401
NXP Employee
NXP Employee

Here is an article regarding to kdump usage:
https://community.nxp.com/docs/DOC-347175

0 Kudos
Reply