How to build fw_printenv and fw_setenv for imx8mq?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to build fw_printenv and fw_setenv for imx8mq?

4,437 次查看
晓锋潘
Contributor I

我在android 9.0.0_2.0.0以及Yocto L4.14.98_2.2.0环境下编译fw_printenv 和 fw_setenv时一直报错,请问有解决方案吗?log如下:

~/i.MX-L4.9.88-2.0.0-Yocto/imx-yocto-bsp/build-xwayland-imx8mqevk/tmp/work/imx8mqevk-poky-linux/u-boot-imx/2018.03-r0/git$ make envtools
scripts/kconfig/conf  --silentoldconfig Kconfig
  CHK     include/config.h
  UPD     include/config.h
  CFG     u-boot.cfg
  GEN     include/autoconf.mk
  GEN     include/autoconf.mk.dep
  CFG     spl/u-boot.cfg
  GEN     spl/include/autoconf.mk
  CHK     include/config/uboot.release
  UPD     include/config/uboot.release
  CHK     include/generated/version_autogenerated.h
  UPD     include/generated/version_autogenerated.h
  CHK     include/generated/timestamp_autogenerated.h
  UPD     include/generated/timestamp_autogenerated.h
  LD      tools/env/built-in.o
  HOSTCC  tools/env/crc32.o
In file included from tools/env/crc32.c:1:0:
tools/env/../../lib/crc32.c:12:10: fatal error: arpa/inet.h: No such file or directory
 #include <arpa/inet.h>
          ^~~~~~~~~~~~~
compilation terminated.
scripts/Makefile.host:116: recipe for target 'tools/env/crc32.o' failed
make[1]: *** [tools/env/crc32.o] Error 1
Makefile:1504: recipe for target 'envtools' failed
make: *** [envtools] Error 2

0 项奖励
回复
3 回复数

3,252 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @wang12zhe ,

 

Create a new case for your question, please!

And our MPU team will take it, and discuss it with you.

I am in charge of WiFi/BT , not support MPU directly.

 

Regards,

weidong

0 项奖励
回复

4,239 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Pan,

   你可以从网上得到很多类似的同行的经验,比如:

https://blog.csdn.net/leochen_career/article/details/81027309 

你之所以编译出错,原因就是makefile中的编译器路径配置不对。

编译这个东西,建议你在linux里编译,先按照linux doc中的一个porting guide 文档描述的standalone模式,把工具链从yocto里导出来。u-boot、kernel代码都整理到一个目录里。当能够用单机模式编译u-boot和内核成功时,单机环境就好用了。

这时候,你再开始编译你的fw_printenv和fw_setenv. 参考上面链接里的经验,编译一下。

或者Yocto里直接编译,我刚刚测试过:

---------------------------

# cd imx-release-bsp

# gedit .build/conf/local.conf

add the line:

IMAGE_INSTALL_append  += " u-boot-fw-utils"   # a space character must be used before "u-boot-fw-utils".

save and exit.

# source setup-environment build

# bitbake u-boot-fw-utils -c compile

# bitbake u-boot-fw-utils -c install

 

Then succeeded.

-------------------------

Have a nice day!

BR,

Weidong

0 项奖励
回复

3,256 次查看
wang12zhe
Contributor III

@weidong_sun 在IMX8QXP上测试,这样操作能 fw_printenv and fw_setenv但 不能用,进入uboot源码编译的却能用,

但怎么自动打包到文件系统能

0 项奖励
回复