Hello,
I download L4.14.98_2.3.0_images_MX8QXPMEK.zip and found it includes Image-imx8qxpc0mek.bin and imx-boot-imx8qxpc0mek-sd.bin-flash imags, but I not found C0xxx binaries after I build BSP according i.MX_Yocto_Project_User's_Guide.pdf of imx-yocto-L4.14.98_2.3.0 document.
How to build C0 version binary for MX8QXPMEK board?
thanks.
已解决! 转到解答。
Hello Ping Wu,
I was reviewing the configuration files and there is a separate MACHINE for each of the two silicon versions supported:
imx8qxpmek for the B0 silicon
imx8qxpc0mek for the C0 silicon
So please bake the recipes you need accordingly. I would recommend having a separate build directory for each instead of using the same one and changing the local.conf file, as to avoid issues when baking.
I hope this information helps!
Regard!
@jordonwu A +
você conseguiu construir uma imagem para o imx8qxpc0mek você pode me passar a receita que usou e as configurações da sua máquina porque estou tentando seguir o guia
de usuário mas sem sucesso estou usando ubunto 20_04-lts-gen2 x64 RAM 16 GiB
Estou com problemas.
Configuração de construção:
BB_VERSION = "2.0.0"
BUILD_SYS = "x86_64-linux
"NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8qxpc0mek"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "5.15-kirkstone"
Resumo: 2 tarefas falharam:/home/johnlcruz/imx-yocto-bsp/sources/poky/meta/recipes-devtools/binutils/binutils-cross_2.38.bb:do_unpack/home/johnlcruz/imx-yocto-bsp/sources/poky/meta/recipes-core/glibc/glibc_2.35.bb:
do_unpack
Hello Ping Wu,
I’m investigating but changes are builds from the Yocto BSP Release would be for the latest revision available at time of release. I will let you know as soon as I have more information.
Regards,
Hello Ping Wu,
I was reviewing the configuration files and there is a separate MACHINE for each of the two silicon versions supported:
imx8qxpmek for the B0 silicon
imx8qxpc0mek for the C0 silicon
So please bake the recipes you need accordingly. I would recommend having a separate build directory for each instead of using the same one and changing the local.conf file, as to avoid issues when baking.
I hope this information helps!
Regard!
Hello gusarambula ,
Great! I Just change machine to imx8qxpc0mek and then build, now there are C0xxx binaries on deploy\images\imx8qxpc0mek folder. Later I will using a separate folder for C0 silicon machine, thanks.
Best Regards