Hi,
I've attached video on how this GStreamer pipeline reproduces V-Sync tearing:
gst-launch-1.0 -v videotestsrc pattern=blink ! video/x-raw,width=1280,height=800 ! autovideosink
Originally I've discovered tearing in Qt 5.15-based QML application, where video is displayed using qmlglsink. we see diagonal tearing in fixed position on top of the screen.
Using fbdevsink in provided pipeline example makes it a bit "better" - the tear is no longer diagonal, just horizontal, but it still exists. But I can't use fbdevsink anyway as video must be composited inside Qt-based interface via qmlglsink...
I've tried various Qt eglfs-related environment variables, but nothing seems to help.
/etc/kms.conf in that device is:
# cat /etc/kms.conf
{
"device": "/dev/dri/card1",
"hwcursor": true,
"pbuffers": true,
"outputs": [
{
"name": "DP",
"mode": "1280x800"
}
]
}
uname -a:
Linux imx8mmevk 5.10.72-lts-5.10.y+gb5085fe8a3ce #1 SMP PREEMPT Tue Oct 25 12:05:04 UTC 2022 aarch64 aarch64 aarch64 GNU/Linux