How to apply new patch to old BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to apply new patch to old BSP

2,719 Views
jasonhsu
Contributor III

Hi Community,

For some aging test issues, I have to apply new patch to old BSP. However, the BSP version on which is the patch based is newer than the BSP I used, if I use the new patch, many conflicts will appear and cannot be fixed manually, because some data structs do not exist at all in old BSP.

We create project last year based on the BSP (IMX6_JB43_110_ANDROID_SOURCE_BSP), see below picture.

16809_16809.jpg1.jpg

and now, I  have to apply new patch (IMX6_JB43_111_ANDROID_SOURCE_BSP) according to FSL FAE suggest, see below picture:

16810_16810.jpg1.jpg

If apply IMX6_JB43_111_ANDROID_SOURCE_BSP to (IMX6_JB43_110_ANDROID_SOURCE_BSP) directly, it will generate many patch failure in kernel_imx. and cannot fix manually, because some data structs do not exist at all.

Could someone teach me how to apply patch based on IMX6_JB43_111_ANDROID_SOURCE_BSP to  (IMX6_JB43_110_ANDROID_SOURCE_BSP) ? many many thxs.

the aging test issue i encouter: Re: Re: Re: V4L2, encoding seems not work.

Best regards,

Jianhua

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

2,508 Views
gusarambula
NXP TechSupport
NXP TechSupport

The JB4.3.0_1.1.1 BSP is not a formal release but a series of patches to be applied on the previous release. Which steps are you following in order to apply these? Please look at section 3.2 of the Android User’s Guide.

It could be possible that some errors occur if modifications were made on the original JB4.3.0_1.1.0. Have you changed the original BSP?

0 Kudos
Reply