How to add opencv lib in eclipse project?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add opencv lib in eclipse project?

1,522 Views
茂实丁
Contributor II

Hello  everybody!

I want add opencv lib in eclipse project ,there are some problems. Could you please tell me the right way to add the library?

I use Ubuntu 14 and solox environment.The Opencv has been compiled.

best regards!

Labels (3)
0 Kudos
Reply
1 Reply

1,367 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Were the recommendations in The problem in building opencv via eclipse
used ?


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply