Hi,
I would like to add a dedicated line as cd-gpios for usdhc1. The pin I connected was MX6QDL_PAD_GPIO_1, so I added
"MX6QDL_PAD_GPIO_1__SD1_CD_B 0x80000000" to structure imx6q-sabrelite in imx6qdl-sabrelite.dtsi file to config the MX6QDL_PAD_GPIO_1 pin for SD1_CD_B function.
But then how I should describe the cd-gpios pin for the usdhc1 device? I saw it all following the same pattern of "cd-gpios = <&gpiox pin level>" for other usdhc device, but since in my situation the pin is a dedicated pin, so I can not follow the same pattern. Can someone help?
Alternatively, should I just add a line of "MX6QDL_PAD_GPIO_1__SD1_CD_B 0x17071" into structure usdhc1 in imx6qdl.dtsi file? just under the existing pin descriptions for usdhc1.
Regards
Damien
已解决! 转到解答。
Hi Igor,
Please don't worry about my question now, it had been fixed.
Instead of setting MAX6QDL_PAD_GPIO_1 to SD1_CD_B, I set it to GPIO1_IO01 with instruction "MAX6QDL_PAD_GPIO_1__GPIO1_IO01 0x17059" in structure imx6q-sabrelite in file imx6qdl-sabrelite.dtsi. And then I use the below structure to describe it within the same file.
&usdhc1 {
pinctrl-names = "default";
pinctrl-0 = <&princtrl_usdhc1_1>;
cd-gpios = <&gpio1 1 0>;
no-1-8-v;
keep-power-in-suspend;
enable-sdio-wakeup;
status = "okey";
};
Log messages from console at boot time now is as below:
"
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: no vqmmc regulator found
mmc0: no vmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
"
Log message from console at the time of SD card insertion is as below:
"
mmc0: host does not support reading read-only switch. assuming write-enable.
mmc0: new high speed SDHC card at address b368
mmcblk0: mmc0:b368 3.73 GiB
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
"
Thanks for your time, igor. It is much appreciated.
Regards,
Damien
Hi Damien
according to linux/Documentation/devicetree..
linux-2.6-imx.git - Freescale i.MX Linux Tree
should be used:
fsl,cd-controller : Indicate to use controller internal card detection
seems below example ["&esdhc1 "
] uses this property
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks igor.
I followed the example you gave to add a structure as below into file imx6qdl-sabrelite.dtsi
&usdhc1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc1_1>;
fsl,cd-controller;
vmmc-supply = <®_3p3v>;
status = "okay";
};
but the machine seems still not able to detect the insertion of a SD card to usdhc1.
below is the log from console in regard to usdhc1 (mmc0) at boot time.
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc-imx 2190000.usdhc: could not get ultra high speed state, work on normal mode
mmc0: no vqmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
and there was nothing output from console when SD card was inserted into slot.
I am wondering how the software knew pin MX6QDL_PAD_GPIO_1__SD1_CD_B was used for card detection but not others. It seems to me there must something missing in this area. do you have more info on this?
Cheers,
Hi Igor,
Please don't worry about my question now, it had been fixed.
Instead of setting MAX6QDL_PAD_GPIO_1 to SD1_CD_B, I set it to GPIO1_IO01 with instruction "MAX6QDL_PAD_GPIO_1__GPIO1_IO01 0x17059" in structure imx6q-sabrelite in file imx6qdl-sabrelite.dtsi. And then I use the below structure to describe it within the same file.
&usdhc1 {
pinctrl-names = "default";
pinctrl-0 = <&princtrl_usdhc1_1>;
cd-gpios = <&gpio1 1 0>;
no-1-8-v;
keep-power-in-suspend;
enable-sdio-wakeup;
status = "okey";
};
Log messages from console at boot time now is as below:
"
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: no vqmmc regulator found
mmc0: no vmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
"
Log message from console at the time of SD card insertion is as below:
"
mmc0: host does not support reading read-only switch. assuming write-enable.
mmc0: new high speed SDHC card at address b368
mmcblk0: mmc0:b368 3.73 GiB
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
"
Thanks for your time, igor. It is much appreciated.
Regards,
Damien