How to add GPIO in imx8mm evk board in dts file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add GPIO in imx8mm evk board in dts file

6,387件の閲覧回数
Ruban1
Contributor II

How to add GPIO in imx8mm evk board in dts file

i want add

MX8MM_IOMUXC_SAI5_RXD3_GPIO3_IO24 0x41

in GPIO

but in imx8mm-evk.dts file i am not able to find  the below function

pinctrl-0 = <&pinctrl_hog_1>;

pinctrl_hog_1: hoggrp-1 {
fsl,pins = <
MX8MM_IOMUXC_GPIO1_IO08_GPIO1_IO8 0x19
MX8MM_IOMUXC_SAI5_RXD3_GPIO3_IO24 0x41

>;
};

 

in which function of the attached .dts file i can add

 

 

i have attached the dts file below

MX8MM_IOMUXC_SAI5_RXD3_GPIO3_IO24 0x41

 

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

6,384件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

6,382件の閲覧回数
Ruban1
Contributor II

Referring  Those  link only i tried to edit but that file is ter in Yocto build . I am working on Android 10 OS.

I dont have such kind of file and ru sure i have to edit in .dtsi file not .dts file 

i have attached screenshot let me know which file i have to edit or add for GPIO

And other screenshot of DTSI file i wil attach the file also .dtsi file let me know where i have to edit or add

Regards

Ruban

0 件の賞賛
返信

6,377件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

for android one can look at

https://github.com/digi-embedded/android-sample-gpio

 

Best regards
igor

 

0 件の賞賛
返信

6,373件の閲覧回数
Ruban1
Contributor II

Its not working the app is getting crashed .

Can  you provide link which can run on Android Studio and library with NXP to access GPIO .

Or just provide in which function i can add GPIO in Android 10 OS and in which file

 

0 件の賞賛
返信

6,365件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

unfortunately I am not aware of NXP similar tool or any documentation related

to gpios in Android, in other words seems "it is not supported". So if you have special need for it

suggest to proceed with help of  https://contact.nxp.com/new-prof-svcs-sw-tech

 

Best regards
igor

0 件の賞賛
返信