How set mx6q_sabresd output the display data to YUV format

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How set mx6q_sabresd output the display data to YUV format

Jump to solution
2,067 Views
kaisun1
Contributor III

HI :

      we use ms6q_sabresd board as a platform to development .  we need the board output the display data  format is 20-bit YCbCr .

Then i read kernel and uboot code .and only find the code what is support HDMI LVDS and RGB  format . what i shoud do ?

Thanks anyway!

1 Solution
1,866 Views
ChucoChe
NXP Employee
NXP Employee

Please check the Linux Release notes table 6. the video section. If the format you want doesn't works in setting by kernel boot parameter. I'm afraid you will have to add it in the kernel or driver.

Michel

View solution in original post

0 Kudos
Reply
3 Replies
1,867 Views
ChucoChe
NXP Employee
NXP Employee

Please check the Linux Release notes table 6. the video section. If the format you want doesn't works in setting by kernel boot parameter. I'm afraid you will have to add it in the kernel or driver.

Michel

0 Kudos
Reply
1,866 Views
kaisun1
Contributor III

Hi michel:

              this proble i have resolve. imx6 is support it .

1,866 Views
kaisun1
Contributor III

HI ,This problem has been solved.   now  i  can output 720P video data.  but 720i  is not work.

0 Kudos
Reply