Hi community,
I have a question about i.MX6SDL eFuse blowing.
Actually, our customer failed eFuse blowing on thier custom board. even though they used PlatformSDK.
The written data was 0x3F3F3F3F though they wrote 0xFFFFFFFF.
But the failure was not occurred on all thier board, a part of their boards were succeeded.
So we doubt current supply for i.MX6.
How much current supply is needed for i.MX6 eFuse blowing?
(e.g. xx mA on VDD_SOC_IN)
Best Regards,
Satoshi Shimoda
已解决! 转到解答。
Hi Satoshi
I am afraid for i.MX6 eFuse blowing current is not specified, but as estimation one can look
i.MX53 data Table 9. Maximal Supply Currents 120mA Fuse Write Mode operation
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX53CEC.pdf
In i.MX6 voltage provided from VDD_HIGH_IN, as described in sect.4.3.2.2 LDO_2P5
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
The LDO_2P5 module implements a programmable linear-regulator function from VDD_HIGH_IN
(see Table 6 for min and max input requirements). Typical Programming Operating Range is 2.25 V to 2.75 V
with the nominal default setting as 2.5 V. The LDO_2P5 supplies the SATA PHY, USB PHY, LVDS PHY,
HDMI PHY, MIPI PHY, E-fuse module and PLLs.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
I am afraid for i.MX6 eFuse blowing current is not specified, but as estimation one can look
i.MX53 data Table 9. Maximal Supply Currents 120mA Fuse Write Mode operation
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX53CEC.pdf
In i.MX6 voltage provided from VDD_HIGH_IN, as described in sect.4.3.2.2 LDO_2P5
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
The LDO_2P5 module implements a programmable linear-regulator function from VDD_HIGH_IN
(see Table 6 for min and max input requirements). Typical Programming Operating Range is 2.25 V to 2.75 V
with the nominal default setting as 2.5 V. The LDO_2P5 supplies the SATA PHY, USB PHY, LVDS PHY,
HDMI PHY, MIPI PHY, E-fuse module and PLLs.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for your reply.
I understood approximately 120mA on VDDHIGH_IN may be needed to program eFuse.
SABRE-SDP design seems to not satisfies this requirement (VGEN5 = max 100mA), so if customer designed same as SABRE-SDP, I think the eFuse programming issue might be occurred by current insufficient.
Beest Regards,
Satoshi Shimoda
Hi Satoshi
1. according to Table 8. Maximum Supply Currents
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
The actual maximum current drawn from VDD_HIGH_IN will be as shown
plus any additional current drawn from the VDD_HIGH_CAP outputs, depending
upon actual application configuration (for example, NVCC_LVDS_2P5, NVCC_MIPI,
or HDMI, PCIe, and SATA VPH supplies).
2. i.MX53 data 120mA is worst case, blowing 8 fuses simultaneously,
blowing 1 fuse bit will require 120/8=15mA (max)
Best regards
igor