How get QuadSPI configuration parameters for IMX6ULL-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How get QuadSPI configuration parameters for IMX6ULL-EVK

1,575件の閲覧回数
黎明周
Contributor I

Hello,everybody

   I have a IMX6ULL-EVK board, want to boot use QuadSPI.I have tried use imgutil tool get  sdk20-app.img in SDK_2.2_MCIM6ULL. reference below

QQ图片20181214101812.png

but can not boot from QSPI,the bin is make by IAR,what is wrong?

      run mfgtool2-sdk20-mx6ul-evk-qspi-nor-n25q256a.vbs ,like these status:

1.png

2.png

3.png4.png5.png

in the last picture,nothing occur forever.why the reminder is "No Device Connected",confirm the usb cabe is connect with board in this process? The  Getting Started with MCUXpresso SDK for i.MX 6ULL Derivatives.pdf is like this

6.png

      

      I see the sdk20-app.img ,it  file contain  IVT, boot data,dcd table ,etc.but didn't contain the boot device configuration parameters.

    I think the img not have device configuration parameters, so can't boot from QSPI,do you think?

   Read IMX6ULLRM.pdf, 

8.6.3 QuadSPI configuration parameters

 this is a table, 512 byte,how to make the table use tool? Is there such a tool?

Thanks.

Regards,

Liming.Zhou

ラベル(1)
0 件の賞賛
返信
1 返信

1,418件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Liming

QuadSPI configuration parameters are provided in

mfg tool folder ..OS Firmware/files (its name like "qspi-nor-micron-n25q256a-config")

Mfg Tool can be found on link

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------