How does yocto enter standby mode by pressing the button

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How does yocto enter standby mode by pressing the button

1,964 Views
fu_qiang
Contributor II

hi ,now we have two buttons on the board, the default is to use one as restart and the other as standby wake-up key, but the standby wake-up key does not work now, which can be understood as how to pick up the hardware now, may I ask whether the YOCto system supports standby wake-up function.The hardware has been connected to GPIO or connected to somewhere.Below is the hardware connection.

pastedImage_1.png

pastedImage_2.png

Bast regards

fu

0 Kudos
Reply
1 Reply

1,873 Views
igorpadykov
NXP Employee
NXP Employee

Hi fu

what processor used in the case, general answer one can find in i.MX Linux Reference Manual

Power Management Chapter, however there may be differencies between

different processors and operating systems.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply