How do MX6ULL use BSP uboot&linux_3.14.52

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do MX6ULL use BSP uboot&linux_3.14.52

604 次查看
shikai
Contributor I

Dear all,

          I have customize a stable MX6UL software version in BSP uboot&linux_3.14.52,  now I need change board to MX6ULL as soon as possible, but I can't find MX6ULL BSP uboot&linux_3.14.52 in imx.git.  

          And I don't want to change BSP to 4.1.15, because the version remove some function in kernel.

          Could you give me some suggestion?

           

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

447 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi kai,

You can refer to the http://cache.nxp.com/assets/documents/data/en/application-notes/AN5350.pdf?fsrch=1&sr=1&pageNum=1 .
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复