How do MX6ULL use BSP uboot&linux_3.14.52

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do MX6ULL use BSP uboot&linux_3.14.52

603 Views
shikai
Contributor I

Dear all,

          I have customize a stable MX6UL software version in BSP uboot&linux_3.14.52,  now I need change board to MX6ULL as soon as possible, but I can't find MX6ULL BSP uboot&linux_3.14.52 in imx.git.  

          And I don't want to change BSP to 4.1.15, because the version remove some function in kernel.

          Could you give me some suggestion?

           

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

446 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi kai,

You can refer to the http://cache.nxp.com/assets/documents/data/en/application-notes/AN5350.pdf?fsrch=1&sr=1&pageNum=1 .
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply