How do I configure imx6q's I2S clock in master mode ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I configure imx6q's I2S clock in master mode ?

3,416 次查看
明镜明
Contributor I

codec works in slave mode, ssi  generate the  sclk and  frame clock .

the sys's clock is 24M,  i follow  the nex table to configure registers :

Table 61-7. SSI Bit Clock and Frame Rate as a Function of PSR, PM, and DIV2. 

but  bit clock and  frame sync clock  dnot work correctly . 

how can i call  function imx_ssi_set_dai_clkdiv according to the sample_rate and sample_format?

 

Do you have relevant document or  demo to introduce  the configure ? 

1502110875.jpg

标记 (1)
0 项奖励
回复
6 回复数

2,968 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 明镜 明

 

for frequency selection examples please refer to Chapter 7
Audio attached Linux Manual and unit tests:

imx-test (folder /mxc_sound_test)
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,968 次查看
明镜明
Contributor I

HI, igorpadykov

       thanks a lot. 

      there is no audio attached Linux manual in  imx-test-5.7.tar.gz.

      how  can i get the audio attached ?

      can you provide for me ?  

0 项奖励
回复

2,968 次查看
igorpadykov
NXP Employee
NXP Employee

sorry, it is ../mxc_sound_test, it is attached.

SDK (../drivers/audio)

swp-report/iMX6_Platform_SDK/sdk/drivers/audio at master · backenklee/swp-report · GitHub 

Best regards
igor

0 项奖励
回复

2,968 次查看
明镜明
Contributor I

HI,igorpadykov

Thanks a lot.

0 项奖励
回复

2,968 次查看
明镜明
Contributor I

HI,@igorpadykov

       Thank you for your answer.

       I  need to configure the i2s clock  in kernel ,not in  app。

      ssi  works in  master mode。

       how can i configur  the ssi‘s register according to  the sample rate and date format.

      in  machine driver (imx-sgtl5000.c)  。

    thanks a lot。

0 项奖励
回复

2,968 次查看
igorpadykov
NXP Employee
NXP Employee

I do not think that this is possible thorugh some simple

register settings using "imx_ssi_set_dai_clkdiv ", as alsa subsystem configures

it using own apis.

Please check attached in previous answer linux manual and

look at sources in Table 7-1. Stereo Codec SoC Driver Files

For better understanding probably may be useful to look at baremetal audio tests

Github SDK (/drivers/audio)
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor

0 项奖励
回复